About OpenCL in L3.14.28_1.0.0.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About OpenCL in L3.14.28_1.0.0.

Jump to solution
494 Views
keitanagashima
Senior Contributor I


Dear All,

Hello.

My customer wants to use the OpenCL in L3.14.28_1.0.0 (i.MX6DQ).

But, OpenCL looks supporting by L3.0.53.

[Question]

Could you tell me the usable OpenCL environment in L3.14.28?

Best Regards,

Keita

Labels (4)
0 Kudos
1 Solution
334 Views
b36401
NXP Employee
NXP Employee

Our OpenCL supposes Linux 3.0.53 kernel and we have no examples or recommendations regarding to 3.14.x.

Sorry for the inconvenience.

However there should not be anything special regarding to 3.14.x kernels.

Have a great day,

Victor
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
335 Views
b36401
NXP Employee
NXP Employee

Our OpenCL supposes Linux 3.0.53 kernel and we have no examples or recommendations regarding to 3.14.x.

Sorry for the inconvenience.

However there should not be anything special regarding to 3.14.x kernels.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos