841-RDFXWIN8USB - is it compatible with Windows 10?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

841-RDFXWIN8USB - is it compatible with Windows 10?

869 Views
shellyrosenfeld
Contributor I

841-RDFXWIN8USB - is it compatible with Windows 10?

Labels (1)
0 Kudos
5 Replies

635 Views
michaelestanley
NXP Employee
NXP Employee

Shelly,

I'll have to do some research to determine the internal sampling interval.

Given the nature of your questions, I think you might want to consider a different platform: specifically our Sensor Fusion for Kinetis MCUs library (nxp.com/sensorfusion) runs on a variety of ARM-based Freedom boards available at nxp.com/freedom.  Full source code is supplied, and you have total control.  The Windows 8 reference design was targeted at OEMs developing Windows-based computers and tablets.  The onlyY defined interface to the module is via the Windows 8 HID standard.

What is your application?

Mike

0 Kudos

635 Views
michaelestanley
NXP Employee
NXP Employee

Shelly,

We haven't requalified against the Microsoft Windows 10 regression suite.  So technically, no.

Regards,

Mike

0 Kudos

635 Views
shellyrosenfeld
Contributor I

Hi,

Thank you for your reply.

Is there a way with RDFXWIN8USB to change the sampling frequency?

The SpWin8View Demo sowtware output a log every 63mSec (15Hz).

As for the accelerometer the MMA8451Q have ODR of 1.56 to 800Hz.

Is there a way to write code and communicate with the with the MCF51Jx: ColdFire?

Thank you,

Shelly

0 Kudos

635 Views
michaelestanley
NXP Employee
NXP Employee

Shelly,

The board is compatible with Microsoft's "HID Sensor Class.

Here is the spec:

https://msdn.microsoft.com/en-us/library/windows/hardware/dn613934(v=vs.85).aspx

You can communicate with the HID sensor using the Accelerometer
class in the Windows.Devices.Sensors namespace. For example, you can change the
sample rate by setting the ReportInterval property.

https://msdn.microsoft.com/library/windows/apps/windows.devices.sensors

The RDFXWIN8USB isn't designed for general development use, but rather as a reference design for the HID interface.  So we're not supplying libraries as part of our general enablement.

Mike

0 Kudos

635 Views
shellyrosenfeld
Contributor I

Hi

Thank you for the information

What is the minimum sampling interval possible?

Is there a way to interrupt the MCU code?

Thanks,

Shelly

0 Kudos