Marvell WIFI firmware init failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Marvell WIFI firmware init failed

3,100 Views
aravinthkumarja
Senior Contributor II

Hi all,

root@green_fs:/system/usr# insmod mlan.ko

root@green_fs:/system/usr# insmod sd8xxx.ko                              

wlan: Loading MWLAN driver

vendor=0x02DF device=0x9119 class="0" function=1

rx_work=1 cpu_num=4

WLAN: FW download, write iomem (0) failed @ 0

wlan_dnld_fw fail ret=0xffffffff

WLAN: Download FW with nowwait: 0

Firmware Init Failed

woal_add_card failed

wlan_sdio: probe of sd:0001:1 failed with error -1

wlan: Driver loaded successfully

root@green_fs:/system/usr#

Firmware location /system/lib/firmware/mrvl/sd8787_uapsta.bin

I don't firmware is taken or not, how to check.

Thanks!

Aravinth

0 Kudos
2 Replies

1,707 Views
igorpadykov
NXP Employee
NXP Employee

Hi aravinthkumar

message "Firmware Init Failed" means that you may need

to contact marvel for updated firmware for that module.

Also may be useful below :

Marvell 8787 based wifi module using SDIO

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,707 Views
aravinthkumarja
Senior Contributor II

Hi igorpadykov,

Thanks for your response, i will check with them.

Thanks!

Aravinth

0 Kudos