Hello. How to sew only MfgTool system.img? The board processor IMX 53 Automotive.
Hello Igor. I wanted to write to you at once, but did not find your email address. I do so, but the program fails. Here is the log:
Friday, March 11, 2016 21:36:38
1 - Panel A Start processing MX53SMD-Android-eMMC4.4 <LIST/>.
Panel A Start <CMD/> type="boot" body="BootStrap" file="u-boot-mx53-smd.bin" timeout="10" onError="" text="Read from DDR script from U-Boot to init DDR Memory.".
1 - Panel A DoBoot() - Failed to load u-boot-mx53-smd.bin to Recovery mode device. (err=6)
1 - Panel A Finished <CMD/> type="boot" body="BootStrap" file="u-boot-mx53-smd.bin" timeout="10" onError="" text="Read from DDR script from U-Boot to init DDR Memory." FAIL code=0x6.
Panel A: Reason is unknown,failed to run command: type="boot" body="BootStrap" file="u-boot-mx53-smd.bin" timeout="10" onError="" text="Read from DDR script from U-Boot to init DDR Memory." 2 - Panel A Finished processing MX53SMD-Android-eMMC4.4 <LIST/> : FAIL code=6.
Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE
2 - Panel A Start processing MX53SMD-Android-eMMC4.4 <LIST/>.
Panel A UtpUpdate Event: DeviceArrival Msg: (null) DevState: BootStrap OpState: OP_UNKNOWN_STATE
Panel A Start <CMD/> type="boot" body="BootStrap" file="u-boot-mx53-smd.bin" timeout="10" onError="" text="Read from DDR script from U-Boot to init DDR Memory.".
2 - Panel A Finished <CMD/> type="boot" body="BootStrap" file="u-boot-mx53-smd.bin" timeout="10" onError="" text="Read from DDR script from U-Boot to init DDR Memory." SUCCESS code=0x0.
Panel A Start <CMD/> type="load" body="" file="uImage" timeout="10" onError="" text="Doing Kernel.".
2 - Panel A Finished <CMD/> type="load" body="" file="uImage" timeout="10" onError="" text="Doing Kernel." SUCCESS code=0x0.
Panel A Start <CMD/> type="load" body="" file="initramfs.cpio.gz.uboot" timeout="10" onError="" text="Doing Initramfs.".
2 - Panel A Finished <CMD/> type="load" body="" file="initramfs.cpio.gz.uboot" timeout="10" onError="" text="Doing Initramfs." SUCCESS code=0x0.
Panel A Start <CMD/> type="jump" body="" file="" timeout="10" onError="" text=" Jumping to OS image. ".
2 - Panel A Finished <CMD/> type="jump" body="" file="" timeout="10" onError="" text=" Jumping to OS image. " SUCCESS code=0x0.
Panel A Start <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="".
Panel A UtpUpdate Event: DeviceRemoval Msg: (null) DevState: Disconnected OpState: WAITING_FOR_DEVICE
Panel A UtpUpdate Event: DeviceArrival Msg: (null) DevState: BootStrap OpState: WAITING_FOR_DEVICE
2 - Panel A Finished <CMD/> type="find" body="Updater" file="" timeout="180" onError="" text="" FAIL code=0xffff0002.
Panel A: Wrong device found.,failed to run command: type="find" body="Updater" file="" timeout="180" onError="" text=""
3 - Panel A Finished processing MX53SMD-Android-eMMC4.4 <LIST/> : FAIL code=-65534.
Hi Oleg
please follow attached document sect.2.8 Build Manufacturing Firmware,
linux on link:
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------