see https://community.freescale.com/thread/320314#comments
processor
Freescale i.MX6SOLO rev1.1 at 792 MHz
It seems this problem is not resolved in kernel 3.10.17. The driver has changed quite a bit, so i don't know if this problem was taken along in the redesign or just not taken up.
Hi vim
3.10.17 is quite old kernel and I am not sure that new patches are
released for it. According to link activity 17.07.2014 15:31, Jeff Horn
produced patch, you can ask it from him. In general recommended to
use latest kernel
Board Support Packages (29)
L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------