In the PRM file, EEPROM_DATA is placed at address 0x800.
EEPROM = READY_ONLY 0x800 To ...
PLACEMENT
...
EEPROM_DATA INTO EEPROM
In th asm file,
EEPROM_DATA :SECTION
byte_800: DS $7A0
DS $5E ; Here if DS $4E is ok
WORD_FFE: DS 2
In the map file,
if Change DS $5E to $4E, can see byte_800 is @addr 0x800, and WORD_FFE is @other address.
but if DS $5E, There is an error, A1102. How can i definition of a var in EE byte_800 at addr 0x800, and WORD_FFE at addr 0xFFE?
Anyone help? Thank you very much.
solve.
i have the wong define of the prm file:
EEPROM = READY_ONLY 0x800 To the last addr of my project.
so it is solve.
Thank you all the same.
What is the architecture used ?
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------