I added some patches to gcc to work around a bug where gcc strips off the leading '/' from include search paths, and "bitbake gcc" worked just fine. When I tried to rebuild my system image, I got the following failure:
ERROR: Function failed: do_configure (log file is located at /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_t4240rdb-64b/tmp/work/ppc64e6500-fsl-linux/web-sysmon/git-r0/temp/log.do_configure.9182)
ERROR: Logfile of failure stored in: /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_t4240rdb-64b/tmp/work/ppc64e6500-fsl-linux/web-sysmon/git-r0/temp/log.do_configure.9182
Log data follows:
| DEBUG: Executing python function sysroot_cleansstate
| DEBUG: Python function sysroot_cleansstate finished
| DEBUG: Executing shell function do_configure
| NOTE: make -e MAKEFLAGS= D=/home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_t4240rdb-64b/tmp/work/ppc64e6500-fsl-linux/web-sysmon/git-r0/image clean
| make: *** No rule to make target `clean'. Stop.
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_configure (log file is located at /home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_t4240rdb-64b/tmp/work/ppc64e6500-fsl-linux/web-sysmon/git-r0/temp/log.do_configure.9182)
ERROR: Task 3886 (/home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale/recipes-extended/web-sysmon/web-sysmon_git.bb, do_configure) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3927 tasks of which 3923 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:
Summary: 1 task failed:
/home/nxp/SDK/QorIQ-SDK-V1.9-20151210-yocto/sources/meta-freescale/recipes-extended/web-sysmon/web-sysmon_git.bb, do_configure
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
nxp@ve:~/SDK/QorIQ-SDK-V1.9-20151210-yocto/build_t4240rdb-64b$
Anyone have any idea what is going on? "bitbake fsl-image-full" worked before the patches, but this seems completely unrelated.
Solved! Go to Solution.
Hello nick caruso,
Please run the command "bitbake web-sysmon -c cleansstate" to build the package web-sysmon from the scratch could help you to overcome this problem.
The compiler has been changed, so all these package and libs should be rebuilt, I suggest you create a new build project and build all the packages(including toolchain) from the scratch.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello nick caruso,
Please run the command "bitbake web-sysmon -c cleansstate" to build the package web-sysmon from the scratch could help you to overcome this problem.
The compiler has been changed, so all these package and libs should be rebuilt, I suggest you create a new build project and build all the packages(including toolchain) from the scratch.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------