Hello.
I'm Working with MPC5645S and code warrior IDE 5.9.
I write a image to external flash memory, and then I try to use the "AHB address" to set the beginning address of layer data. (DCU.LAYER[6].CTRLDESCL3.R = 0x70000000)
However, the image is not read correctly, it seems that the MPC5645 is not fast enough to read the data . Should we active the DMA mode?
Please could you send an example code that use an external flash memory to save images?
Thanks,
Josep Gorgues
Hi,
take a look at this application note, section 3 and especially section 3.2:
http://www.nxp.com/files/microcontrollers/doc/app_note/AN4865.pdf
External Quad SPI flash memory can be relatively slow for some display resolutions.
Regards,
Lukas