qt5 not running if kernel build outside of the yocto project with version changes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

qt5 not running if kernel build outside of the yocto project with version changes

508 Views
narasimhuluorug
Contributor III

Hello,

Any one can suggest where I am missing as below mentioned log. Here I am working with 3.14 kernel and building separately but in qt5 yocto project of fsl is some another kernel version. Please suggest any inputs.

:~# qt5demo-starter

QEglFSImx6Hooks will set environment variable FB_MULTI_BUFFER=2 to enable double buffering and vsync.

If this is not desired, you can override this via: export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1

[     1] HAL user version 5.0.11 build 19959 Aug  6 2014 03:02:58

[     2] HAL kernel version 5.0.11 build 25762

Segmentation fault

Best Regards,

Narasimha

0 Kudos
1 Reply

292 Views
jimmychan
NXP TechSupport
NXP TechSupport

could you tell me why not build all the things together in yocto?

0 Kudos