Hi, I'm having issues with this chip.
Found odd behavior of the NXP switch, the output voltage is 1V less than the input if the load is Hi-Z.
Also found that the output voltage gets limited to 3.5V with constant load and increasing voltage.
I read in the datasheet that the Input and output voltages can be 0 to 5.5V, so why am I experiencing this limiting?
Thanks,
Victor