automotive-grade Linux on i.mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

automotive-grade Linux on i.mx6

1,995 Views
liyingchun
Contributor I

Hi expert

I use i.mx6UL for a automotive application. I want to know that:

(1) Does NXP(fsl) provide the automotive-grade Linux for I.mx6?

(2)  I notice that more that one doc on your web site mention that freescale can provide automotive-grade Linux to customer, you can see them: http://cache.nxp.com/files/32bit/doc/fact_sheet/LINUXFS.pdf?fromsite=zh-Hans&fsrch=1&sr=3&pageNum=1%...

http://cache.nxp.com/files/automotive/doc/brochure/PRFSRVCSAUTPBRCH.pdf?fromsite=zh-Hans&fsrch=1&sr=...

and I know that NXP(fsl) is the member of Automotive Grade Linux (AGL), you can see https://www.automotivelinux.org/

My qestion is that if the automotive-grade Linux provided by freescale is the open sourced Linux Distribution by (AGL)?

Thanks!

Labels (1)
0 Kudos
3 Replies

806 Views
igorpadykov
NXP Employee
NXP Employee

Hi li

I am not aware of i.mx6 nxp automotive-grade linux releases, but it may be useful

to contact local marketing for obtaining more information.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos

806 Views
liyingchun
Contributor I

Hi igor

Thanks for your reply, do you or anyone know some information about NXP automotive-grade linux releases? even if it does not support I.mx6.

For example, Does NXP still release(sustain) the automotive-grade linux? what platform the automotive-grade linux support? Thanks!

0 Kudos

806 Views
CarlChien
NXP Employee
NXP Employee

Hi li,

Regarding AGL, one demo is under NXP git sever. See http://git.freescale.com/git/cgit.cgi/imx/meta-nxp-agl.git/.

For details, you can refer to README http://git.freescale.com/git/cgit.cgi/imx/meta-nxp-agl.git/tree/README.txt?h=krogoth

 

Please note it’s demo, provided “as is”.

Thanks and Best regards,

Carl

 

0 Kudos