AnsweredAssumed Answered

SPC5634MF1MLQ80 burning interface of application is not successful, request to assist analysis

Question asked by JACK li on Feb 25, 2016

We have for your company's SPC5634MF1MLQ80 TQFP144 microcontroller in burning program, through a number of times there are some material software don't burn in!

Has not been tried two ways respectively, burn write success

Using CodeWarrior IDE v2.10 and OSJTAG debugger to burn (interface such as attachment 1)

USES MPC chip bringing the Bootloader program written BDM mode, through RS232 burning (burning failure interface as shown in attachment 3), RS232 model for: TEK ZE551A

OSJTAG烧写程序不成功界面截图.pngOSJTAG烧写工具.jpg

rs232烧写界面截图1.png

我司在对贵司的SPC5634MF1MLQ80,TQFP144单片机烧录程序时,通一批次其中有部分物料软件烧录不进去!

  分别尝试了两种方式,均未烧写成功

采用CodeWarrior IDE v2.10和OSJTAG调试器进行烧录(失败界面如附件1)

采用MPC芯片自带的BDM模式编写的Bootloader程序,通过RS232烧写(烧写失败界面如附件3所示),RS232型号为:TEK  ZE551A

 

 

以上异常请协助分析什么原因。谢谢!

 

 

 

The above abnormal please help analysis the reason why.Thank you very much!

Outcomes