i.MX6Q/EEPROM Recovery

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q/EEPROM Recovery

Jump to solution
691 Views
soichiyamamoto
Contributor V

Hi,

There is EEPROM Recovery Enable in 8.5.5.1 Serial ROM eFUSE Configuration of i.MX 6Dual/6Quad Applications Processor Reference Manual.

Is this flag a function to perform what concretely?

Best Regards,

soichi

Labels (2)
0 Kudos
1 Solution
417 Views
Yuri
NXP Employee
NXP Employee

Hello,

From section 8.9 (Recovery Devices) of the RM :

"The Chip supports recovery devices. If primary boot device fails, boot ROM will try to

boot from recovery device using one of I2C or ECSPI ports.

For enabling recovery device BOOT_CFG4[6] fuse must be set. Additionally Serial

EEPROM fuses must be set as described in Serial ROM through SPI and I2C."


Have a great day,
Yuri
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
418 Views
Yuri
NXP Employee
NXP Employee

Hello,

From section 8.9 (Recovery Devices) of the RM :

"The Chip supports recovery devices. If primary boot device fails, boot ROM will try to

boot from recovery device using one of I2C or ECSPI ports.

For enabling recovery device BOOT_CFG4[6] fuse must be set. Additionally Serial

EEPROM fuses must be set as described in Serial ROM through SPI and I2C."


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos