AnsweredAssumed Answered

I am looking into replacing the 'end of life" WindRiver Probe with the CodeWarrior TAP.  So I have downloaded an eval version of CodeWarrior for Networked Applications. In my first attempt to create a bare-metal project I observe the "Debug Target Setting

Question asked by samedwards on Feb 25, 2016
Latest reply on Feb 26, 2016 by samedwards

I am looking into replacing the 'end of life" WindRiver Probe with the CodeWarrior TAP.  So I have downloaded an eval version of CodeWarrior for Networked Applications. In my first attempt to create a bare-metal project I observe the "Debug Target Settings" only present Freescale's own p1010RDB, RDB-PB eval/development boards to choose from. My application has a custom board, and I merely want to port the existing board-bring up code. So is there a simple way to create a project without the CodeWarrior's presumption that Freescale boards are the only selection?

Outcomes