Hi
I would like to use two GPIO pins on the imx6qdl-sabrelite board to implement some relay liked activity.
That is one pin as an input, the other pin as output. Once the input pin becomes active, I would like to invert it and output to the output pin.
Can this be implemented with the existing device tree without needing a new driver on the kernel?
Cheers,
Damien
Hi Damien
I am afraid this is not possible, so software code should be added
for such purpose.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------