MPC5777C, TSENS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C, TSENS

614 Views
ameyaranade
Contributor II

Hello All,

 

I am trying to read the on chip temprature sensor. To calculate the temprature value i Need the Parameters TSCA and TSCB from the UTEST Memory. If i understand correct, the values are located at 0x00400000, 0x00400002, 0x00400004 and 0x00400006.

In my case but i those Flash Locations are unprogrammed and i am reading 0xFFFF for all the Parameters.

Am i missing something?

 

Thank you all.

Labels (1)
Tags (2)
0 Kudos
1 Reply

460 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

It sounds like you have pre-production part and it is possible, and very likely, that it does not have anything programmed into UTEST.

Here is the data I read from device I have (PPC5777CMM0, 2N45H)

Address                Data

0x00400000         0x00CF0007

0x00400004         0x00940013

BR, Petr

0 Kudos