Hello all,
I'm using an example freertos project that for the k64F series(KSDK1.2) and made some minor changes to it to make it run on the twr-k64f120m board and it runs fine.
I'm trying to implement code that uses queues to communicate between tasks.to that end I created 4 tasks:
I changed heap_3 to heap_1
However now my code is generating a trap.
As I said I'm kind of new to freertos and I'm certain there are lots of mistake in the code.
My code is trying to creat 4 tasks :
void task_one(task_param_t param);
void task_two(task_param_t param);
void vATask(task_param_t param);
void vADifferentTask(task_param_t param);
The main.c is attached .The vATask is entered and successfully post the value of the variable it is pointing, to the queue however as soon it returns ,I hit a trap of some kind.
I'm using KDS. the disassembly window shows WD_ HANDLER as the trap but the C source window shows the default ISR which basically are the same thing which is just spinning for ever. I believe it is the hard_fault exception.
Thanks,
Koorosh Hajiani
Original Attachment has been moved to: main.c.zip