Yuri Muhin

Re: Linux iMX6 PCIe driver not working

Discussion created by Yuri Muhin Employee on Dec 2, 2015
Branched from an earlier discussion
Branched to a new discussion

Hello,

 

  Please check PCIe clock configuration.

 

HW Design Checking List for i.Mx6DQSDL Rev2.9 contains useful recommendations

about using (external) PCIe clock :

"Due to CLKx_P/N is LVDS port and don't match with PCIe reference clock specification.

For PCIe Gen1 application, following low cost solution can be used(DC bias and AC

impedance should be considered).  Please refer to "HW Design Checking List for i.Mx6DQSDL

Rev2.7.xlsx", sheet "Schematic", Ref12 for more info."

 

  "PCIe reference clock solution which provided by CLKx_N/P of i.MX6 chip can't pass PCIe

Gen2 compliance test.  Recommend using external PCIe 2.0/3.0 clock generator with 2 HCSL

outputs solution. One clock channel connect to i.MX6 as a reference input, please click

Ref14 ("HW Design Checking List for i.Mx6DQSDL Rev2.9.xlsx") for reference circuit.

Another clock channel should connect to PCIe connector, please contact generator vendor

for detailed design guide."

 

HW_Design_Checking_List_for_i.MX6DQP6DQ6SDL 


Have a great day,
Yuri

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Outcomes