Hi,
I have a Sabre SD board that passes calibration consistently. When I try to run
the graphical stress tester 2.4 the first address fails as follows:
address of failure 0x1000 0000
Data was: 0x10000008
But pattern should match address
Error: failed to run stress test!!
I am setting the start frequency to 350mhz and 525 for the end.
Any help would be appreciated. I am doing this in preparation for testing
my custom board of similar design to the Sabre SD.
Thanks!
Larry
Original Attachment has been moved to: ddr_calibration_20160222-15'37'28.log.zip
Hi Larry
from log: "ddr_mr1=0x00000000 " -
MR1 should be set to meaningful value.
In script examples MR1=4 set in init script like:
setmem /32 0x021b001c = 0x00048031 // MMDC0_MDSCR, MR1 write, CS0
The MR1 value is upper 4 hex bits written to MMDCx_MDSCR
Also one can run ddr test without gui, it has mr1 in script text
i.MX6 DDR Stress Test Tool V1.0.3
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------