Hi,
I need a help .I am trying to boot Android 5.0.2 lollipop on imx6sl evk.i tried prebuild image also but i getting following error .please help me out.
EXT4-fs (dm-0): mounted filesystem with ordered data mode. Opts: barrier=1
fs_mgr: __mount(source=/dev/block/dm-0,target=/system,type=ext4)=0
EXT4-fs (mmcblk1p4): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk1p4): recovery complete
EXT4-fs (mmcblk1p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
fs_mgr: __mount(source=/dev/block/mmcblk1p4,target=/data,type=ext4)=0
EXT4-fs (mmcblk1p6): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk1p6): recovery complete
EXT4-fs (mmcblk1p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
fs_mgr: __mount(source=/dev/block/mmcblk1p6,target=/cache,type=ext4)=0
EXT4-fs (mmcblk1p7): mounted filesystem with ordered data mode. Opts: (null)
fs_mgr: __mount(source=/dev/block/mmcblk1p7,target=/device,type=ext4)=0
binder: 120:120 transaction failed 29189, size 0-0
init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead
init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead
init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead
init: cannot find '/system/bin/debuggerd64', disabling 'debuggerd64'
init: cannot find '/system/bin/install-recovery.sh', disabling 'flash_recovery'
android_usb: already disabled
mtp_bind_config
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
binder: 147:147 transaction failed 29189, size 0-0
Original Attachment has been moved to: lollipop_kernel_struck.zip
Hi aravinthkumar
may be you used wrong image, please try to write sd card with
mfg tool using mfgtool2-android-mx6sl-evk-sd.vbs script
Programmers (Flash, etc.) (9)
IMX-L5.0.0-MFG-TOOL (REV L5.0.0_1.0.0)
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------