Looking for Silicon tuner RFin(400MHz) to IF(30-60MHz)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Looking for Silicon tuner RFin(400MHz) to IF(30-60MHz)

722 Views
yossidruyan
Contributor I

Hello,

I'm looking for Silicon tuner in the RF 400MHz similar to TDA18214 or TDA18250, but with IF output of 30MHz to 60MHz,Pls advise.

Thanks,

Yossi Druyan

Given Imaging,Medtronic

Labels (1)
0 Kudos
1 Reply

525 Views
soledad
NXP Employee
NXP Employee

Hello Yossi Druyan,

For terrestrial TV reception, we recommend either the TDA18272 or TDA18273. Both can receive legacy analog signals, digital transmission according to worldwide adopted standards, and digital cable signals.

8PSK satellite tuners TDA20136 and TDA20142 are recommended for TVs that need digital satellite reception, and especially those that receive Free to Air (FTA) satellite services.

For applications that require sensitivity and noise figure beyond what’s already integrated into NXP’s high-performance silicon tuners, an external LNA from the BGU703x or BGU704x series can be used in front of the terrestrial or cable tuner.

Find more Silicon Tuners in the following link:

Silicon Tuners|NXP


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos