hi all,
have anyone tried usb mfs code with FRDM-k64f with mqx4.2 and codewarrior 10.6.....please let me know if it is working....for me it is showing errors.
thanks.
Hello shweta karade,
I suggest to clone your own libraries. You can take as base the twrk60f120m BSP and use the BSPCloningWizard.
The twrk60f120m BSP includes the USB legacy and you can work with codewarrior 10.6
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello shweta karade,
MQX includes two USB stacks:
The example code located at the path C:\Freescale\Freescale_MQX_4_2\mfs\examples\mfs_usb
illustrates the usage of USB host (legacy USB stack).This example doesn't support theFRDM-K64F.
What example are you using?
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
am using example from mqx 4.1 for frdm k64f with mqx 4.2.. as u
mentioned "Legacy
USB stack with minor changes and bugfixes. Includes support for legacy
platforms only (same processors previously supported in MQX RTOS 4.1.1.) "in
mqx 4.1 it supports FRDM k64f...so i thought it wil work in mqx4.2
also....so can u suggest any other example code for frdm k64f platform with
mqx 4.2 and codewarrior 10.6
thanks
On Mon, Feb 22, 2016 at 7:53 PM, soledad <admin@community.freescale.com>