Unable to boot with nitrogen6x board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to boot with nitrogen6x board

635 Views
madhureddy
Contributor I

Hello all,

Currently am working with nitrogen6x board.

Earlier the device was booting, by mistakenly i did something in u-boot environment, now it is not booting.

showing the below information and after that it is stopping.

U-Boot 2014.07-00136-gf870252 (Sep 22 2014 - 09:16:34)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

Reset cause: WDOG

Board: Nitrogen6X

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

SF: Detected SST25VF016B with page size 256 Bytes, erase size 4 KiB, total 2 MiB

auto-detected panel wvga-rgb

Display: wvga-rgb (800x480)

In:    serial

Out:   serial

Err:   serial

Net:   using phy at 6

FEC [PRIME], usb_ether

U-Boot >

Please help on this it is very urgent.

0 Kudos
1 Reply

514 Views
gary_bisson
Senior Contributor III

Hi Madhu,

It looks like you've either erased the bootcmd varialble or set bootdelay to -1 which disables autoboot.

My advice, clear your saved environment:

> env default -a

> saveenv

> reset

Regards,

Gary

0 Kudos