AnsweredAssumed Answered

Debug views in KDS 3.0.0

Question asked by Frank Schuetz on Feb 19, 2016
Latest reply on Feb 19, 2016 by David E Seymour

Hello,

I use KDS 3.0.0 with TWR-K65F180M and KSDK 1.3.0. On debugging there are several  views to monitor internal of MQX.

My question is, some views show no information and less show a message like "MessagePool is not installed"(see screen attached). What is to do that I get these information. Is something to install on KDS or on software side on K65?

I have seen that the view for "MQX LightWheight Memory Pools" are available (see screen attached) but I use the MQX as in your example projects and I thinks (I'm sure) it is configured as MQX light weight. It is correct so as it is?

 

Another question is, I have seen that the "MQX LightWheight Memory Pools" show a size of 127,3KB. We use the internal RAM (256KB) only (no external RAM). I think that is a lot! I this the size what the MQX heap is used? When I use MQX-LightWheigt is it more less? How much do you think? Actually we have problems with the less memory heap with our application and want to save heap.

 

Thank you in advance!

Outcomes