Hello.
I am starting to use the KSDk with KL25Z microcontroller.
and reading the sample project i could see that the structure they use for this configuration is this one
osc_user_config_t osc0Config = { .freq = OSC0_XTAL_FREQ, .hgo = MCG_HGO0, .range = MCG_RANGE0, .erefs = MCG_EREFS0, .enableCapacitor2p = OSC0_SC2P_ENABLE_CONFIG, .enableCapacitor4p = OSC0_SC4P_ENABLE_CONFIG, .enableCapacitor8p = OSC0_SC8P_ENABLE_CONFIG, .enableCapacitor16p = OSC0_SC16P_ENABLE_CONFIG, }; CLOCK_SYS_OscInit(0U, &osc0Config);
but if you look at the SDK reference manual the order is different.
as i am new both are right?
osc_user_config_t osc0Config = { .freq = OSC0_XTAL_FREQ, .enableCapacitor2p = OSC0_SC2P_ENABLE_CONFIG, .enableCapacitor4p = OSC0_SC4P_ENABLE_CONFIG, .enableCapacitor8p = OSC0_SC8P_ENABLE_CONFIG, .enableCapacitor16p = OSC0_SC16P_ENABLE_CONFIG, .hgo = MCG_HGO0, .range = MCG_RANGE0, .erefs = MCG_EREFS0, }; CLOCK_SYS_OscInit(0U, &osc0Config);
Solved! Go to Solution.
Hello Edri,
They are both ok, the two structures includes the same members ,
there is no matter about the sequence.
Hope it helps
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Edri,
They are both ok, the two structures includes the same members ,
there is no matter about the sequence.
Hope it helps
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------