AnsweredAssumed Answered

iMX6UL 24 MHz crystal oscillator

Question asked by Riccardo Manera on Feb 18, 2016
Latest reply on Feb 19, 2016 by Riccardo Manera

Hello,

 

I've developed our custom board based on iMX6UL and I've a question about workaround suggest in Chip errata, ERR009455:

what happen if the pin XTAL IN is left floating (point 1) ) without connecting a 18pF load? Does the iMX6UL boot up correctly?

Reading the IMX6ULHDG document, it seems that a capacitor in the XTALIN pin is needed only for filtering.

Thanks in advance

Riccardo

Outcomes