Hi,
I would like to use the MC9S12XEQ512MAL to generate a CAN frame (without receive one). Indeed I have to to wake up an IC with a specific CAN frame.
I made several try without success......
I don't have the frame expected at MCU pin number 104 (txcan0).
Would like, please, help me on this issue ? Maybe you have a code ready to use to obtain the CAN frame with this version of S12X.
Many thanks.
Hi Mohamed,
The simple example code is in attachment.
More examples are for example here:
LAMA's S12XE unofficial examples
The “official” msCAN driver:
http://www.nxp.com/files/microcontrollers/software/device_drivers/MSCAN_S12_DEVD.zip
I hope it helps you.
Have a great day,
RadekS
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------