I've created sato image with chromium using fsl-community-bsp. However, when I launch it from desktop, the device reboots.
GitHub - Freescale/chromium-imx mentions that you have to use --use-gl=egl. I'm not sure if the desktop link is providing this.
Should this cause the device to reboot if this was the case though?
I'm thinking, if I build x11 image should I be able to run chromium with this option. Has anyone else been able do this before?
Hello,
You may try NXP BSP - please refer to section 5.6.6 (Chromium Browser on X11,
XWayland and Wayland) of "Freescale_Yocto_Project_User's_Guide.pdf".
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------