We have an application that we are looking at the i.MX 7D for. The issue that I would like some clarity on is the 2x USB OTG ports. Our application requires a dual-device functionality. This means that our system can be hooked up to two hosts at the same time via the OTG. The need for this is uninterrupted transfer when changing hosts. Is the i.MX7D capable of performing this?
Hi Adam
2x USB OTG ports can work simultaneously in Device mode.
What means "uninterrupted transfer when changing hosts" ?
There is no special i.MX capability, they work as usual two USB Device.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------