custom 2G DRAM u-boot for mfgtools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

custom 2G DRAM u-boot for mfgtools

1,138 Views
tootzoe
Contributor III

my custom board with 2G DRAM now runs very well,  see  how to change ddr to 2G on u-boot 2015.04

next i need to make a u-boot for mfgtools.

my android is 5.1.1,  the mfgtools is different from previous  versions, i followed thd document <Manufacturing Tool V2 Linux or Android Firmware Development Guide V2.docx> to modify the header file mx6sabresd.h (my board based on sabresd-6q),  added the below code:

#define CONFIG_MFG

#define CONFIG_CMDLINE_TAG

#define CONFIG_REVISION_TAG

#define CONFIG_SETUP_MEMORY_TAGS

#define CONFIG_INITRD_TAG

#undef  CONFIG_BOOTDELAY

#define CONFIG_BOOTDELAY 0

#define CONFIG_ENV_IS_NOWHERE 1

#undef CONFIG_BOOTARGS

#undef CONFIG_BOOTCOMMAND

#define CONFIG_BOOTARGS "console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 " \

  "g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off"

#define CONFIG_BOOTCOMMAND      "bootz 0x12000000 0x12c00000 0x18000000"

#undef CONFIG_EXTRA_ENV_SETTINGS

#define CONFIG_EXTRA_ENV_SETTINGS \

  "splashpos=m,m\0"  \

  "fdt_high=0xffffffff\0"  \

  "initrd_high=0xffffffff\0" \

  "bootcmd_mfg=bootz 0x12000000 0x12c00000 0x18000000\0"

compile , got u-boot.imx,  this bin file ready for mfgtools, i reuse original zImage and initramfs and dtb files,  just replace the u-boot located  mfgtools\Profiles\Linux\OS Firmware\firmware,  the mfgtools burns roms for my custom board successfully. everything runs good.

Labels (1)
0 Replies