AnsweredAssumed Answered

OHCI context controller active bit doesn't clear

Question asked by H VO on Feb 15, 2016
Latest reply on Feb 16, 2016 by Pavel Chubakov

I'm having a problem running on the T2080 that when I transmit to a PCIe by setting the OHCI context controller run bit, the context controller active bit is set and remains set (never clears!)  The active bit is set and cleared only by the Host Controller. 

Can someone tell me why this is the case?  This piece of code runs fine on the T1040.

thanks!

Outcomes