Hi,
I purchase MotoHawk ECM‐S12X‐070‐1001. I was told that CodeWarrior for HCS12(X) Microcontrollers, v4.6 is the only compiler I can use to build the software.
I have a PC with Win7 Pro, Matlab 2014b and MotoHawk 2014b sp2. I wonder if v4.6 works with Win7, or it's just works with WinXP.
I wonder if this setup in the PC can work with the ECM.
Thanks
Zhen
Hi,
In addition to my previous message.
I've re-installed CW for HC12 v4.6 on my Win 7 64 bit OS.
After to have build the project I've tried to launch the debugger.
You can got an error when the debugger is launched.
In some case you need to re-specifiy the path of debugger tool:
On my side I got some errors when I launch the debugger and the application is not loaded.
Similar project using same configuration (Hardware) is working fine with HC12 V5.1
Is there a problem with the P&E plugins used on HC12 V4.6 ?
Download the Patch for (S)12(X) 3rd Party Software, unzip it and refer to the readme.txt file.
On my side I backup the \Codewarrior for HC12 V4.6\Prog folder and extracted all files contained in the downloaded zip file.
After that I was able to launch the debug session and download the code on board using my P&E USBMultilink interface.
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi
CW for HC12 V4.6 is an old version released in 2006.
This tool was fully tested on Win XP 32 bit OS.
To avoid problem we recommend to use it under XP os.
CW for HC12 V5.1/V5.2 are lasted versions and these were tested under Host Platforms:
HC12 V4.6 under Win 7 ?
Sometimes ago I've performed some installation test see below:
+++++++++++++++++++++++++++++++++++++++++
Launch the CW12_V4_6.exe
Next
Next
and
Next + Next + Next + Next
Select Complete and click on Next + Next and
Install
The installation is launched.
An error message appears
This is linked to a driver issue (P&E)
Click on OK and a second message
Click on OK
Click on OK
The installation is rolling back
And …
The tool is not installed.
Executed exactly the same process excepted for the Setup type, select custom
Next
Remove the driver from installer
Click on Next + Next + install
CW for HC12 V4.6 is now installed
Finish
Go to the P&E web site:
http://www.pemicro.com/products/product_viewDetails.cfm?product_id=33
Click on FAQs, Manuals & Downloads Tab
Under Download select: P&E Hardware Interface Drivers, Version 11 (Win XP/Vista/7/8)
PEDrivers_install.exe
Launch the installer
P&E drivers are installed.
+++++++++++++++++++++++++++++++++++++++++
At this point, the tool is installed.
I will check on my side how the tool is running (license) and debugger.
Not sure if it will work fine under Win 7.
Have a great day,
Pascal
NXP Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------