AnsweredAssumed Answered

MPC5606B BAM Serial Communication

Question asked by fscheidl on Feb 6, 2016
Latest reply on Feb 8, 2016 by Lukas Zadrapa

I just read about the included Boot Assist Module in MPC5606B. I understand that I have to set the FAB and ABS pins accordingly to disable booting from internal flash and make use of the Boot Assist Module instead.

 

Is the LINFlex_0 module set to UART mode automatically when I set the FAB and ABS pins accordingly?

Is it correct that I have to use the LINFlex_0 module in order to communicate with the MCU in BAM status?

For booting from CAN, I guess the relevant pins/module is FlexCAN_0 (CAN0TX, CAN0RX) then?

 

Thank you very much in advance!

Outcomes