AnsweredAssumed Answered

SoC/TRx 2.4 GHz  for bluetooth  and  proprietary protocols

Question asked by Tobias Drößler on Feb 5, 2016
Latest reply on Feb 5, 2016 by Tobias Drößler

Hi anyone.

 

I am looking for a hardware plattform (RF-TRx or Sytem on chip) for a bigger project, which can be act as an bluetooth (low energy)  node  -- and on the other hand can be configured to handle a simple proprietary protocoll  (without all  the BT features),  its for compatibility mode.  

 

both configurations are independent, so the are two different firmwares.

 

best regards / nice weekend

Outcomes