Hi All,
I have downloaded Android Lollipup v5.1.1 for i.MX6 Sololite, and flashed it on to the card and booted, I observed that some binder is failing.
PFA by name error_after_booting.jpg, and while flashing the card it says /dev/sdb5 is not a block special device PFA by name while_flashing.png.
This issue is not seen while flashing with Android 4.4.3 earlier.
Please help me to proceed further.
Thanks and Regards,
Joseph vikas.
Please find the image for the above post in which command line is not accessible.
Thanks & Regards,
Joseph Vikas.
Hi vikas,
System image is not mounted.
This is my log:
Below 2 line is not coming in your log.
EXT4-fs (mmcblk3p5): mounted filesystem with ordered data mode. Opts: barrier=1
fs_mgr: __mount(source=/dev/block/mmcblk3p5,target=/system,type=ext4)=0
EXT4-fs (mmcblk3p4): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk3p4): mounted filesystem with ordered data mode. Opts: nomblk_io_submit,noauto_da_alloc,errors=panic
fs_mgr: __mount(source=/dev/block/mmcblk3p4,target=/data,type=ext4)=0
EXT4-fs (mmcblk3p6): Ignoring removed nomblk_io_submit option
EXT4-fs (mmcblk3p6): mounted filesystem with ordered data mode. Opts: nomblk_io_submit
fs_mgr: __mount(source=/dev/block/mmcblk3p6,target=/cache,type=ext4)=0
EXT4-fs (mmcblk3p7): mounted filesystem with ordered data mode. Opts: (null)
fs_mgr: __mount(source=/dev/block/mmcblk3p7,target=/device,type=ext4)=0
init: Starting service 'logd'...
Hope above information is helpful for you!
Regards,
Aravinth
Hi All,
I have generated binaries by building the android lollipup source v5.1.1. When I flashed them on to sd card and booted, I
can get access to GUI, but I am unable to access command line. I have tried the prebuilt images also which resulted the same.
I am using MFG tool to flash the images on to the sd card.
Please help me to move forward.
Thanks and Regards,
Joseph Vikas.