i.mx6dl - Log significance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx6dl - Log significance

524 Views
dipalidhumal
Contributor I

Hi,

These are panic logs from i.mx6dl processor.

Please let us know these logs are related to which module or device. -

Please revert if require more information.

:CAP_PXPMemFree:140 page_size = 4[<8002d2a8>] (warn_slowpath_fmt+0x30/0x40) from [<80327ae8>] (dma_release_from_contiguous+0xbc/0x100)

096    buf_size = 1843200

[<80327ae8>] (dma_release_from_contiguous+0xbc/0x100) from [<802d85a4>] (pxp_free_dma_buffer+0x44/0x50)

[<802d85a4>] (pxp_free_dma_buffer+0x44/0x50) from [<802d8eb8>] (pxp_device_ioctl+0x520/0x944)

[<802d8eb8>] (pxp_device_ioctl+0x520/0x944) from [<800d5734>] (do_vfs_ioctl+0x80/0x5bc)

[<800d5734>] (do_vfs_ioctl+0x80/0x5bc) from [<800d5cac>] (SyS_ioctl+0x3c/0x5c)

[<800d5cac>] (SyS_ioctl+0x3c/0x5c) from [<8000ea80>] (ret_fast_syscall+0x0/0x30)

---[ end trace 94c4e7e0c6b4f1c4 ]---

------------[ cut here ]------------

WARNING: at mm/page_alloc.c:6047 dma_release_from_contiguous+0xbc/0x100()

112 pages are still in use!

Modules linked in: wl18xx(O) wlcore(O) mac80211(O) cfg80211(O) wlcore_sdio(O) compat(O)

CPU: 0 PID: 653 Comm: transformerHD.o Tainted: G        W  O 3.10.53 #186

[<80014668>] (unwind_backtrace+0x0/0x138) from [<80011eb0>] (show_stack+0x10/0x14)

[<80011eb0>] (show_stack+0x10/0x14) from [<8002d1f8>] (warn_slowpath_common+0x4c/0x68)

[<8002d1f8>] (warn_slowpath_common+0x4c/0x68) from [<8002d2a8>] (warn_slowpath_fmt+0x30/0x40)

[<8002d2a8>] (warn_slowpath_fmt+0x30/0x40) from [<80327ae8>] (dma_release_from_contiguous+0xbc/0x100)

[<80327ae8>] (dma_release_from_contiguous+0xbc/0x100) from [<802d85a4>] (pxp_free_dma_buffer+0x44/0x50)

[<802d85a4>] (pxp_free_dma_buffer+0x44/0x50) from [<802d8eb8>] (pxp_device_ioctl+0x520/0x944)

[<802d8eb8>] (pxp_device_ioctl+0x520/0x944) from [<800d5734>] (do_vfs_ioctl+0x80/0x5bc)

[<800d5734>] (do_vfs_ioctl+0x80/0x5bc) from [<800d5cac>] (SyS_ioctl+0x3c/0x5c)

[<800d5cac>] (SyS_ioctl+0x3c/0x5c) from [<8000ea80>] (ret_fast_syscall+0x0/0x30)

---[ end trace 94c4e7e0c6b4f1c5 ]---

------------[ cut here ]------------

WARNING: at mm/page_alloc.c:6047 dma_release_from_contiguous+0xbc/0x100()

112 pages are still in use!

Modules linked in: wl18xx(O) wlcore(O) mac80211(O) cfg80211(O) wlcore_sdio(O) compat(O)

CPU: 0 PID: 653 Comm: transformerHD.o Tainted: G        W  O 3.10.53 #186

[<80014668>] (unwind_backtrace+0x0/0x138) from [<80011eb0>] (show_stack+0x10/0x14)

[<80011eb0>] (show_stack+0x10/0x14) from [<8002d1f8>] (warn_slowpath_common+0x4c/0x68)

[<8002d1f8>] (warn_slowpath_common+0x4c/0x68) from [<8002d2a8>] (warn_slowpath_fmt+0x30/0x40)

[<8002d2a8>] (warn_slowpath_fmt+0x30/0x40) from [<80327ae8>] (dma_release_from_contiguous+0xbc/0x100)

[<80327ae8>] (dma_release_from_contiguous+0xbc/0x100) from [<802d85a4>] (pxp_free_dma_buffer+0x44/0x50)

[<802d85a4>] (pxp_free_dma_buffer+0x44/0x50) from [<802d8eb8>] (pxp_device_ioctl+0x520/0x944)

[<802d8eb8>] (pxp_device_ioctl+0x520/0x944) from [<800d5734>] (do_vfs_ioctl+0x80/0x5bc)

[<800d5734>] (do_vfs_ioctl+0x80/0x5bc) from [<800d5cac>] (SyS_ioctl+0x3c/0x5c)

[<800d5cac>] (SyS_ioctl+0x3c/0x5c) from [<8000ea80>] (ret_fast_syscall+0x0/0x30)

---[ end trace 94c4e7e0c6b4f1c6 ]---

Regards,

Dipali

Tags (1)
0 Kudos
1 Reply

343 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dipali

in log there are references to PxP and uSDHC (sdio, wl18x) so you can pay

attention to these drivers.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos