AnsweredAssumed Answered

,b4860qds ethernet interface speed

Question asked by Victor Gomez on Feb 3, 2016
Latest reply on Feb 4, 2016 by ufedor

Hi All,

 

I have one b4860qds board currently working. There are three Ethernet ports in it: J16 (100Mbps), J18 and J20 (both 1000Mbps). The only one working by default is J16, which is the 100Mbps, ergo the slower one.

 

How can I enable J18 or J20 so that I can work with them as well? Does that depend on the BSP of the OS I am running? I am currently running VxWorks 653 2.5 and I wonder if this is something I need to tell to the BSP guys or something I can do directly in the board.

 

Thanks a lot!

Outcomes