GPMI and BCH in IMX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

GPMI and BCH in IMX6UL

494 Views
x10
Contributor V

Hi all,

Both GPMI and BCH are missed in the system memory map (table 2-1 iMX6UL RM), but the related chapters about them contain mapping information. Are these info right or not?

Thanks for answer.

BR

Cheng Shi

Emtronix

Labels (2)
0 Kudos
1 Reply

350 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The GPMI and BCH are included in APBH DMA area in Table 2-1
(System memory map) of the i.MX6UL RM.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos