AnsweredAssumed Answered

i.MX6SL NVCC33_IO.

Question asked by Satoshi Shimoda on Feb 3, 2016
Latest reply on Feb 3, 2016 by Yuri Muhin

Hi community,

 

I have a question about i.MX6SL NVCC33_IO.

When I hear the symbol name NVCC33_IO, I feel I can supply 3.3V to NVCC33_IO pad.

However, the operating range is min 2.8V, typ 3.0V, max 3.3V.

I think, this spec is not wrong, and the symbol name should be NVCC30_IO to be exact.

Is this correct?

 

Or NVCC33_IO spec is wrong?

(e.g. min 1.65V typ 3.3V max 3.6V)

 

Best Regards,

Satoshi Shimoda

Outcomes