Is the bootloader included by factory default in MK20DX128VFM5 MCU?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is the bootloader included by factory default in MK20DX128VFM5 MCU?

446 Views
tatanmejia
Contributor I

I am developing a system based on the FRDM-K64F. Watching the schematics (http://cache.nxp.com/files/microcontrollers/hardware_tools/schematics/FRDM-K64F_SCH.pdf​) I noticed that the OpenSDA interface uses the MK20DX128VFM5 MCU as programming and debugging drive. If I buy the MK20DX128VFM5 MCU, it has the bootloader included by Factory default?

Labels (1)
0 Kudos
1 Reply

301 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Jhonatan Mejía:

Actually no, the MK20DX128VFM5 does not have the OpenSDA firmware loaded from factory. In the next document there is a description of OpenSDA and there is also a binary file attached to program the bootloader to the K20:

OpenSDAv2

I hope this helps.

Regards!

Jorge Gonzalez

0 Kudos