Hello,
I'm running Kernel 3.14.28 on a custom imx6q-based board and I'm having the following problem with the GPU:
[galcore]: GPU[0] hang, automatic recovery.
Once recovery is complete things work. Anyway, recovery causes HMI unavailability...
I have two questions:
1. What is going on with the GPU to have a GPU hang?
2. Is there some recent change/patch which addresses this problem?
Thank you.
Salvatore
Hello,
You may try the recent BSP L3.14.52, where GPU driver is upgraded to Vivante v5.0.11p7.4.
http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS
Summary Page :
i.MX 6 Series Software and Development Tool|NXP
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------