AnsweredAssumed Answered

X T-2080 QDS Board vs. fsl_t2080_qds in vxWorks 6.9 BSP

Question asked by Daeil Kang on Feb 1, 2016
Latest reply on Feb 1, 2016 by Pavel Chubakov

Dear All

 

I want to use fsl_t2080_qds BSP in the vxWorks 6.9 version with X T-2080 QDS board without any modification.

The board says the below information.

SCH-28012 REV A4

700-28012 REV A

X-T2080-QDS

 

The vxWorks 6.9 BSP says the below information.

SCH-28012 REV A3

700-28012 Rev X6

Freescale XT2080QDS

 

I programmed the default bootrom into X-T2080-QDS board.

But it doesn not work, I could see nothing on the serial terminal.

 

Can I use this vxWorks 6.9 BSP with this QDS board?

 

If no, please let me know which part is different between QDS board and this vxWorks BSP.

 

Thanks in advance

Kang

Outcomes