T4240rdb disabling congestion management at DPAA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T4240rdb disabling congestion management at DPAA

791 Views
sedat_altun
Contributor III

Is there any way to disable congestion management while using DPAA  at T4240rdb with SDK 1.9 .

My problem is after an ingress packet rate, the forwarding packet rate of T4240 is dropping dramatically.

I suspect there is an congestion control for the ingress traffic and this is the reason of performance degradation.

Any help will be appreciated.

Best regards

Labels (2)
Tags (2)
0 Kudos
1 Reply

504 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Sedat Altun,

Please configure FSL_DPAA_INGRESS_CS_THRESHOLD in Kernel configuration file.

This parameter is Ingress congestion threshold on FMAN ports. The size in bytes of the ingress tail-drop threshold on FMan ports. Defaults to 0x10000000. Traffic piling up above this value will be rejected by QMan and discarded by FMan.

In addition, please check the congestion information with debugfs.

# mount -t debugfs none /sys/kernel/debug/

root@p4080ds:~# cat /sys/kernel/debug/fsl_dpa/eth0

DPA counters for fm1-gb1:

CPU irqs rx tx recycle confirm tx sg tx err ...

0/0 5 2 2 0 3 0 0

1/1 6 2 0 0 4 0 0

2/2 6 5 4 0 1 0 0

3/3 6 2 1 0 4 0 0

4/4 6 5 12 0 1 0 0

5/5 6 2 0 0 4 0 0

6/6 6 4 3 0 2 0 0

7/7 6 3 0 0 3 0 0

Total 47 25 22 0 22 0 0

Device congestion stats:

Device has been congested for 0 ms.

CGR id 0 avg count: 0

Device entered congestion 0 times. Current congestion state is: not congested.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos