AnsweredAssumed Answered

modifying bsp fails

Question asked by Niklas Roth on Jan 29, 2016
Latest reply on Feb 5, 2016 by soledad

Hi,

 

I set up a new MQX project and drag and droped the bsp and psp for my tower into the worksapce.

(C:\Freescale\Freescale_MQX_4_2\mqx\build\cw10gcc\...\..._twrk60d100m.wsd)

 

Because I want to connect to the onboard accelerometer, I used the processor expert to add the library for the i2c interface. After generating the codes and recompiling the bsp the following error occurres:

 

C:/Freescale/Freescale_MQX_4_2/mqx/source/io/debug/iodebug_asm.S:58: Warning: ignoring changed section attributes for .text

 

And I have no idea how to handle this!!?? Has anyone else an idea?

 

bsp_problem1.png

Outcomes