I am using CodeWarrior Development Studio for S12(X) 5.1 for a 9X12XE128 processor. It appears the serial monitor is not supported on the X processors. I see an old post that says they are not (yet) supported. Is that correct or am I doing something wrong? Any plans if the future?
Hi,
we have an4258 for S12(X)
http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4258.pdf
here is demo code:
http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4258SW.zip
9X12XE128 demo code is also included in the package.
can this help you?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you, that information is interesting and potentially useful but the question was: Does CodeWarrior support the serial monitor to the 9S12XE processors and if not, is there any plans to support it. I presume the answer to both questions is "no" but just wanted to confirm. Thanks.
hi
CodeWarrior 5.1 is the exact ide that can support 9s12x family well, so 9s12xe is also included.
Best regards.
Jennie