Unused eSDHC Interface Pin Recommendations in P1022 Processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unused eSDHC Interface Pin Recommendations in P1022 Processor

403 Views
prasantahalder
Contributor II

It is specified in P1022 design checklist that if eSDHC interface is not used SDHC_DAT0/GPIO1_[25], SDHC_DAT[1:2], SDHC_DAT3 should be configured as GPIO Output, leave floating. But SDHC_DAT[1:2] pins cannot be configured as GPIO output. What should be recommendation for unused SDHC_DAT[1:2] pins?

Labels (1)
Tags (1)
0 Kudos
1 Reply

292 Views
Pavel
NXP Employee
NXP Employee

If pins are configured as SDHC, tie to inactive state through 10–100kpull-up resistors.

It is common practice. To ensure reliable operation, it is highly recommended to connect unused inputs to an appropriate signal level.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos