Murata wifi couldn't work!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Murata wifi couldn't work!

2,490 Views
oliverkuo
Contributor IV

Hi all,

 

We have a i.MX6 Dual board with Murata LBEE5KL1DX and couldn't work properly.

Below error message always showed when driver trying to bring up wifi.

<4>dhdsdio_htclk: HT Avail timeout (1000000): clkctl 0x50

<4>dhd_bus_init: clock state is wrong. state = 1

The BSP is IMX6_L5.1_2.1.0_AND_SOURCE_BSP.

Attached please find kernel log and dts file!

Any idea about this issue?

 

Best regards,

Oliver

Original Attachment has been moved to: imx6q-gr60mxd.dts.zip

Original Attachment has been moved to: murata_1dx_03.log.zip

Labels (2)
Tags (3)
0 Kudos
4 Replies

863 Views
igorpadykov
NXP Employee
NXP Employee

Hi Oliver

please install Broadcom firmware package for i.MX Linux L3.14.52 BSP (REV L3.14.52)

21 Dec 2015

NXP Sign In | Register

also suggest to post on Murata support imxfaq@murata.com, as updated firmware may be

needed for module

Wi-Fi Bluetooth for Freescale i.MX | RF Modules | Wireless Products | Murata Manufacturing

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

863 Views
oliverkuo
Contributor IV

Hi igor,

I'm trying to get support from Murata, before they respond where can I find "Broadcom firmware package for i.MX Linux L3.14.52 BSP (REV L3.14.52)

21 Dec 2015"?

You provide a sign-in link, but I can't find any useful information after sign-in!?

Per your statement, not only Boradcomm firmware package need to be installed but also the firmware of module have to be updated?

Or they are the same thing?

Best regards,

Oliver

0 Kudos

863 Views
skaicai
Contributor I

I have the same problem, Do you solved this question ? If so can you plz tell how to do kindly.

0 Kudos

863 Views
oliverkuo
Contributor IV

Hi,

You may just need a proper Broadcom firmware package for your BSP.

Best regards,

Oliver

0 Kudos