I'm using DS-5 starter edition version: 5.23.1 with FRDM-KL25Z as OpenSDA interface. Enumeration and driver installation in Windows 7 worked without issues. In Device Manager board is shown as Jungo Connectivity: PEMicro OpenSDA Debug Driver with additional OpenSDA - CDC Serial Port.
I'm using bare metal MQX application on CM-4 core. Target connection is CMSIS-DAP but when I click Browse under Connections no devices can't be found. Did someone have same issue? I did search for any kind of OpenSDA problem but nothing was related to this that could solve my problem. Bootloader was upgraded, tried with other versions but nothing. Board information is at the end of post.
If someone is using same configuration, can you please post connection string so I can try entering manually?
Information about device found on PEMicro site is:
Board Name is: FRDM-KL25Z
MicroBoot Kernel Version is: 1.05
Bootloader Version is: 1.11
Installed Application: PEMicro Debug App
Application Version is: 1.08
Hello vjekoslavdelimar,
I'm afraid DS-5 doesn't support the FRDM-KL25Z. If you want to use this board you can use CodeWarrior 10.6 CodeWarrior Software Development Tools|NXP
or KDS Kinetis Design Studio Integrated Development |NXP
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------