AnsweredAssumed Answered

3.14.28-1.0.0_ga: bitbake meta-toolchain-qt5 does not produce "widgets"

Question asked by Durmuş Kurtuluş on Jan 26, 2016
Latest reply on Jan 26, 2016 by Durmuş Kurtuluş

Hello community,

 

I downloaded L3.14.28_1.0.0_iMX6QDLS_BUNDLE and followed the steps in Freescale Yocto Project User's Guide.

I bitbaked "fsl-image-qt5" and then "meta-toolchain-qt5". I did QtCreator setup and tried to build my application.

Immediately I got "QMainWindow: no such file or directory" error.

When I looked inside the sdk image, indeed there is no qmainwindow.h file. In fact QtWidgets was not included in the image.

 

I created a qtbase_5.3.2.bbappend inside fsl-release-bsp/sources/meta-qt5/recipes-qt/qt5 with the following:

PACKAGECONFIG_append = " widgets"

 

But it did not work. I still get the same sdk image.

 

What can i do to include QtWidgets in the toolchain?

 

Thanks in advance.

Durmus

Outcomes