[imx6] RS422 could be supported on Imx6 series ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[imx6] RS422 could be supported on Imx6 series ?

Jump to solution
1,157 Views
keres_kim
Contributor II

HI Developers ~

Good days ~~

simple question. Imx6 chipset could support RS422 serial communication ?

Reference manual said that imx6 support rs232 and rs485, but Nothing mentioned to rs422.

That is why I wonder rs422 could be supported or not.

Does anyone know rs422 on imx6, please leave your comment below ~~

Thank you.

0 Kudos
1 Solution
870 Views
igorpadykov
NXP Employee
NXP Employee

Hi keres

RS422 can be used with i.MX6, standard only defines signal levels so

one can use RS232 to RS422 converter

RS-422 - Wikipedia, the free encyclopedia

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
871 Views
igorpadykov
NXP Employee
NXP Employee

Hi keres

RS422 can be used with i.MX6, standard only defines signal levels so

one can use RS232 to RS422 converter

RS-422 - Wikipedia, the free encyclopedia

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
870 Views
keres_kim
Contributor II

Hi Igor,

Thank you for your answer.

You're right. imx6 works well with RS422 transmiter.

TX is working well, But Still RX(from PC to target) is not.

Do you have any idea ? I just type like "cat /dev/ttymxc3" and wait the data, but nothing comes in.

0 Kudos